You configure the time span of a trend chart x-axis to display the records that are recorded within a specific period of time.
In WorkStation, in the System Tree pane, select the trend chart you want to configure.
On the Trend Chart toolbar, click the Open trend chart settings button
In the Time mode box, select Absolute (start and end time) .
In the Start time boxes, type the x-axis leftmost date and time.
In the End time boxes, type the x-axis rightmost date and time.
Click OK .
The x-axis is now configured with an absolute time span.