You copy a backup set to the Local (db_backup) folder to restore the targeted Enterprise Server or Enterprise Central.
In WorkStation, in the System Tree pane, select the Enterprise Server or Enterprise Central you want to configure.
Click the Control Panel tab.
Click Backup and Restore Manager .
In the Backup sets path box, copy the entire backup sets path of the Enterprise Server or Enterprise Central.
Open a browser, such as Windows Explorer.
In the browser Address box, paste the backup sets path and press Enter .
In the db_backup folder, open the LocalBackup folder.
Right click the backup set that you want to copy and click Copy .
Navigate to the db_backup folder of the Enterprise Server that you want to restore.
Paste the backup set into the LocalBackup folder of the targeted Enterprise Server.
If the LocalBackup folder does not appear within the db_backup folder, you can create one using the exact name, LocalBackup .
You can now restore the Enterprise Server or Enterprise Central using this backup set. 有关更多信息,请参阅 Restoring the EcoStruxure BMS Server .