earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Localization
Product version: 1.9
12/14/2016

Creating a Custom Time Zone of a SmartStruxure Server

If your time zone is not listed in Predefined time zone , you create and configure a custom time zone for the SmartStruxure server.

Show More
action_close

​A time zone is a region on the earth that has a uniform standard time, usually referred to as the local time. Local time is the UTC time plus the current time zone offset for the considered location. Some time zones also have an offset called DST added during the summer period. The DST offset is typically +1 hour.

Network Time

​Consistent date and timestamping across a network is critical for system wide access control, security, communications, scheduling, alarms, and events. Network time uses the NTP protocol that provides the correct current UTC time.

For more information, see Network Time .

Time and Time Zone Configuration in WorkStation

​In WorkStation, all times are by default displayed in local time. This means that a time, independent of its source, is displayed in the same time zone as the operating system on which WorkStation is installed. By configuring the operating system time and time zone settings, you configure how times are displayed in WorkStation. For more information, please refer to the manufacturer’s manual for the operating system.

For more information, see Time and Time Zone Configuration in WorkStation .

Time and Time Zone Configuration in Enterprise Server

​The Enterprise Server time and date settings are configured through the operating system settings on which the Enterprise Server is installed. The time zone offset, configured through the Enterprise Server, is added by Building Operation to the UTC time. The Enterprise Server time zone settings are therefore independent of the operating system time zone settings.

For more information, see Time and Time Zone Configuration in Enterprise Server .

Time and Time Zone Configuration in SmartStruxure Server Device

​To adjust the SmartStruxure server device time, time zone, and DST, you have to access the SmartStruxure server device through a WorkStation.

For more information, see Time and Time Zone Configuration in Automation Server .

To customize a time zone of a SmartStruxure server
  1. ​On the Tools menu, click Control Panel .

  2. ​On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. ​Click Network time and time zones.

  4. Select Custom time zone .

     
    action_zoom_plus_stroke
  5. In the Description box, type a description of the time zone.

  6. In the UTC offset box, select in hours and minutes the time zone offset from UTC.

    Note:
    • The UTC offset is positive east of Greenwich. For example, the time offset for Eastern Time is UTC -05:00 hours.

  7. Select This custom time zone uses daylight saving time to have the time zone automatically updated for daylight saving time.

  8. In the Time adjustment box, select the daylight saving time offset in minutes.

  9. In the Start column, select the month, week, day, and time the daylight saving time starts.

  10. In the End column, select the month, week, day, and time the daylight saving time ends.

  11. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Time and Time Zone Configuration in Enterprise Server
  • Enterprise Server – Date & Time View
  • Changing the Time Zone of a SmartStruxure Server