Funkcje: Trendy
Wersja produktu: 3.2, 3.3, 2022
2021-07-20

Creating a Manual Trend Log

You create a manual trend log that records data that you manually enter.

Pokaż więcej
action_close

​The manual trend log records data that you manually enter. The manual trend log does not log a variable. Use this type of trend log when values from offline devices have to be manually registered to the trend log. For example, if you want to create a trend log that monitors an electricity meter that cannot be connected to the EcoStruxure BMS.

The default size of a manual trend log is 100 records.

 
action_zoom_plus_stroke Manual trend log schematic.
Rysunek: Manual trend log schematic.
Manual trend log meter functionality

A manual trend log can be created with initial meter settings. The manual trend log supports the meter change command and meter consumption calculation. You can view the last meter change information on the manual trend log object. Więcej informacji zawiera Meter Function .

To create a manual trend log
  1. In WorkStation, in the System Tree pane, select the folder or EcoStruxure BMS server where you want to create the trend log.

  2. On the File menu, point to New , and then click Trend .

  3. In the Create Object wizard, in the object type list, select Manual Trend Log.

  4. In the Name box, type a name for the trend log.

  5. In the Description box, type a description.

  6. Click Next .

  7. In the Configure Manual Log page, in the Unit box, click Browse button.

  8. In the Select Unit dialog box, select a unit for the trend log values.

  9. In the Prefix box, select the prefix of the unit.

  10. Click Select .

  11. Click Next .

  12. In the Initial Meter Settings page, in the Set initial meter box, select True to enable the meter function.

  13. In the Start time box, enter the time when the meter was installed.

  14. In the Start value box, enter the value of the new meter when it was installed.

  15. In the Min value box, enter the first value of the new meter after roll-over.

  16. In the Max value box, enter the last value of the new meter before roll-over

  17. Clilck Next .

  18. In the Connect Objects to the Trend Log page, in the Extended Trend Log box, click the Browse button to create an extended trend log and connect it to the trend log.

  19. In the Trend Log List box, click the Browse button to create a trend log list and connect it to the trend log.

  20. In the Trend Chart box, click the Browse button to either create a new trend chart or connect the trend log to an existing trend chart.

  21. Click Create .

The manual trend log is created in the selected folder. You have to manually add the records to the manual trend log.

  • Manual Trend Logs
  • Create Object Dialog – Naming the Object Page
  • Create Manual Trend Log Wizard – Configure Manual Log Page
  • Create Trend Log Wizard – Initial Meter Settings Page
  • Create Trend Log Wizard – Connect Objects to the Trend Log Page
  • Adding a Trend Log Record to a Manual Trend Log
  • Trend Units
  • Meter Function
  • Creating an Extended Trend Log
  • Creating a Trend Log List
  • Creating a Trend Chart that Monitors a Trend Log Series