功能: 趋势
产品版本: 1.8
2016/10/13

Creating a Manual Trend Log

You create a manual trend log that records data that you manually enter.

显示更多
action_close

​The manual trend log records data that you manually enter. The manual trend log does not log a variable. Use this type of trend log when values from offline devices have to be manually registered to the trend log. For example, if you want to create a trend log that monitors an electricity meter that cannot be connected to Building Operation.

 
action_zoom_plus_stroke Manual trend log schematic.
图: Manual trend log schematic.

To create a manual trend log
  1. In WorkStation, in the System Tree pane, select the folder or SmartStruxure server where you want to create the trend log.

  2. On the File menu, point to New , and then click Trend .

  3. Select Manual Trend Log.

     
    action_zoom_plus_stroke
  4. In the Name box, type a name for the trend log.

  5. In the Description box, type a description.

  6. Click Next .

  7. In the Unit box, click browse button

     
    action_zoom_plus_stroke
    .

     
    action_zoom_plus_stroke
  8. Select a unit for the trend log values.

     
    action_zoom_plus_stroke
  9. In the Prefix box, select the prefix of the unit.

  10. Click Select .

  11. Click Next .

  12. In the Extended Trend Log box, click the Browse button

     
    action_zoom_plus_stroke
    to create an extended trend log and connect it to the trend log.

     
    action_zoom_plus_stroke
  13. In the Trend Log List box, click the B rowse button

     
    action_zoom_plus_stroke
    to create a trend log list and connect it to the trend log.

  14. In the Trend Chart box, click the Browse button

     
    action_zoom_plus_stroke
    to either create a new trend chart or connect the trend log to an existing trend chart.

  15. Click Create .

The manual trend log is created in the selected folder. You have to manually add the records to the manual trend log.

  • Manual Trend Logs
  • Adding a Trend Log Record to a Manual Trend Log
  • Trend Units
  • Creating an Extended Trend Log
  • Creating a Trend Log List
  • Creating a Trend Chart that Monitors a Trend Log Series