You create a multistate schedule to control the state of a multistate value.
In WorkStation, in the System Tree pane, select the SmartStruxure server or the folder where you want to create the schedule.
On the File menu, point to New and then click Schedule .
In the object type list, select Multistate Schedule .
In the Name box, type a name for the schedule.
In the Description box, type a description for the schedule.
Click Create .
Now you can add events to the multistate schedule and bind it to a multistate value.