You create a user account group to make it easier to manage users who require the same software permissions and workspaces.
In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.
Click the Control Panel tab.
Click Account management .
In the Domain box, select the domain where you want to create the user account group.
In the User Account Groups area, click Add .
In the Create Object wizard, in the Name box, type a name for the user account group.
In the Description box, type a description for the user account group.
Click Next .
In the Users Belonging to this Group page, in the Select from box, select a user account group to auto select the user accounts belonging to that group in the Available User Accounts list.
In the Available User Accounts list, select the user accounts you want to add to the user account group.
Click the Add button
Click Next .
In the Workspaces Belonging to this Group page, in the Select from box, select a user account group to auto select the workspaces assigned to that group in the Selected Workspaces list box.
In the Available Workspaces box, select the workspaces you want to add to the user account group.
Click the Add button
Click Next .
In the Windows Group Name and Group Policies page, select Allow members to close WorkStation if you want the users in the user account group to be able to close the WorkStation software.
Select Log user actions of group members if you want to activate logging for the users in the user account group.
Select Allow members to change password if you want the users in the user account group to be able to change their own passwords.
Select Allow members to access AS Web Configuration if you want the users in the user account group to be able to log on to SmartX servers' Web configuration sites.
In the Automatic logoff box, select a time if you want the users in the user account group to be logged off after a defined time of inactivity. Para obtener más información, consulte Automatic Logoff .
Select On logoff switch to guest account if you want to log on to the guest account when user accounts that belong to the user account group are manually or automatically logged off. Para obtener más información, consulte Automatic Logoff to Guest Account .
Click the refresh button
To connect a Windows Active Directory user account group to an EcoStruxure Building Operation user account group, you need to establish the connection between the EcoStruxure Building Operation domain and Active Directory Windows domain. Para obtener más información, consulte Creating and Configuring a Domain .
Windows Active Directory account groups can only be mapped on EcoStruxure BMS servers that are running on Microsoft Windows operating system. SmartX servers cannot map Windows Active Directory groups.
In the Windows group name box, select the Windows Active Directory user account group you want to map to the EcoStruxure Building Operation user account group.
You can map Windows Active Directory universal and global account groups to EcoStruxure Building Operation user account groups, but you cannot map Windows Active Directory domain local user account groups.
Click Create .