earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: User Management
Product version: 1.8, 1.9
3/16/2016

Creating a User Account

You create a user account when you want a person to have access to Building Operation.

Show More
action_close

Using WebStation, you can create and administer user accounts.

You can also add a new user account to an already existing user group in the system. You can force users to change their password the next time they log on. Unused accounts can be disabled and saved for further use or they can be deleted from the system.

To create a user account
  1. In WebStation, in the System Tree pane, expand System .

  2. Expand Domains and then expand the domain where you want to create the user.

  3. Right-click User and then click New user .

  4. In the User name box, type the user name.

     
    action_zoom_plus_stroke

  5. In the First name box, type the first name.

  6. In the Middle name box, type the middle name.

  7. In the Last name box, type the last name.

  8. In the Home email box, type the home email address.

  9. In the Work email box, type the work email address.

  10. In the Password box, type the password.

  11. In the Confirm password box, type the password again.

  12. In the Expiration box, enter the expiration date for the user account.

  13. Select User must change password at next logon to force the user to change the password the next time the user log on.

  14. Select Account is disabled to disable the account.

  15. In the Member of box, select which user groups you want the user to be a member of.

  16. Click the Apply button

     
    action_zoom_plus_stroke
    .

  • Create and Administer User Accounts in WebStation
  • Forcing Users to Change Their Passwords
  • Disabling a User Account
  • Deleting a User Account