earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Localización
Versión del producto: 1.9
14/12/2016

Date and Time Properties – Time Tab

Use the Time tab to configure the network time server addresses or establish a lead and shadow relationship on SmartStruxure servers.

 
action_zoom_plus_stroke Time tab
Figura: Time tab

Tabla: Time Tab

Component

Description

Use external NTP server

Select Enabled to define the primary and secondary NTP server addresses for connected shadow SmartStruxure server devices.

NTP Server 1

​Type the address to the primary time server to which the shadow SmartStruxure server devices date and time object synchronizes its clock.

NTP Server 2

Type the address to the secondary time server to which the shadow SmartStruxure server devices date and time object synchronizes its clock.

Lead object

​Enter the object that acts as the lead for this object.

NTP Server 1 Key Id

Type the ID of the authentication key for the primary time server.

NTP Server 2 Key Id

Type the ID of the authentication key for the secondary time server.

Password

Type the password for the primary time server.

Confirm Password

Type the password for the primary time server again.

Password

Type the password for the secondary time server.

Confirm Password

Type the password for the secondary time server again.

Authenticate Network Time Synchronization

Select if you want to use authenticated network time synchronizing.

  • Network Time
  • Synchronize Network Time Settings
  • Enterprise Server – Date & Time View
  • Date and Time Properties – Basic Tab