earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebReports
Functionalities: Reports
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Deleting a Report Schedule

You delete a report schedule when you want to remove the schedule from your schedule list.

Show More
action_close

WebReports Schedules provide a way for you to automatically generate a dashboard report at specified times and days. You create a report schedule using the Schedules menu option at the WebReports Web site.

Using the Schedules settings, you can perform the following tasks:

  • Create a schedule

  • Edit a schedule

  • Specify the frequency for running the scheduled report

  • Specify start dates and times for running the schedule

  • Select a format for the scheduled report output

  • Select a destination for the scheduled report output

  • Disable a schedule temporarily

You can only schedule dashboard reports with Schedules. For more information, see Dashboard Reports .

Report Schedule Frequency

You can specify how often you want a schedule to run, for example weekly or monthly, or perhaps just once.

For more information, see Report Schedule Frequency .

Report Schedule Modifications

You can copy the settings of one schedule and use them to provide the settings for another schedule, when you want to run a different scheduled report.

For more information, see Report Schedule Modifications .

To delete a report schedule
  1. In WebReports, on the menu bar, click Schedules .

  2. In the Select existing schedule list, select the schedule that you want to delete.

  3. Click Delete .

  4. Click OK .

  • Dashboard Reports
  • Schedules for Dashboard Reports
  • Report Schedule Modifications
  • Creating a One Time Only Report Schedule
  • Creating a Daily Report Schedule
  • Creating a Weekly Report Schedule
  • Creating a Monthly Report Schedule
  • Editing a Report Schedule
  • Disabling a Report Schedule