Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 2.0, 2.1, 3.0, 3.1
21/02/2023

Displaying an Alarm View when an Alarm is Triggered

You configure the built-in Alarm pane to automatically open an Alarm View dialog box in a new window when an alarm is triggered.

To display an Alarm View when an alarm is triggered
  1. In WorkStation, in the built-in Alarms pane, right-click anywhere to display the context menu.

  2. Point to Alarm View settings and then click Display Alarm View on alarm .

  • Creating a Filtered Alarm View
  • Alarms Pane and Alarm View Customization
  • Alarm View Properties
  • Menú contextual del panel de Alarmas - Submenú Ajustes de visualización de alarmas