earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 2.0, 2.1, 3.0, 3.1
16/01/2019

Alarms Pane and Alarm View Customization

You use the Alarms pane and the Alarm View to view and administer alarms. When an alarm is triggered, it is displayed in the Alarms pane or Alarm Views together with information about the alarm. You can edit the Alarm View filter to display the Alarm View only when certain alarms are triggered. You can create and use more than one Alarm View. The Alarms pane and each Alarm View can be customized with an alarm filter to show information that is relevant to the user who supervises the alarms. Customized settings are lost when you perform a system upgrade.

In the Alarms pane and Alarm Views, you can also open a detailed view to inspect all properties for a selected alarm.

 
action_zoom_plus_stroke The Alarms pane
Figura: The Alarms pane

Through Control Panel, you can customize the appearance of different alarm states that are displayed in the Alarms pane and Alarm Views. For example, you can change the font style, font size, background color, and font color.

You can also configure the alarm to flash or play a sound when it is triggered.

Alarm View standard filter and layout

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users of the the EcoStruxure BMS.

Para obtener más información, consulte Alarm View and Event View Standard Filter and Layout .

  • Alarms Overview
  • Barra de herramientas del panel Alarmas y la vista Alarma
  • Alarms Pane and Alarm View Icons
  • Alarm Styles View
  • Styling the Alarm States in the Alarms Pane and Alarm Views
  • Acknowledged Style Properties
  • Alarm Style Properties
  • Disabled Style Properties
  • Fault Style Properties
  • Reset Style Properties
  • Displaying an Alarm View when an Alarm is Triggered
  • Creating a Filtered Alarm View
  • Panel Alarmas y vista Alarma
  • Cambio de la ordenación de los estados de alarma
  • Creating a Filtered Alarm View
  • Alarm View Properties
  • Alarm View and Event View Standard Filter and Layout
  • Saving an Alarm View Standard Layout
  • Editing an Alarm View Standard Filter
  • Resetting the Alarm View Standard Layout to Factory Default
  • Ajustar el ancho de la columna al contenido
  • Seleccione el cuadro de diálogo Condiciones
  • Cambio de la ordenación de los estados de alarma
  • Cuadro de diálogo de ordenamiento de estados de alarma
  • Displaying Milliseconds in Alarm Views
  • Alarm Control Panel Synchronization