Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2023-02-21

Displaying an Alarm View when an Alarm is Triggered

You configure the built-in Alarm pane to automatically open an Alarm View dialog box in a new window when an alarm is triggered.

To display an Alarm View when an alarm is triggered
  1. In WorkStation, in the built-in Alarms pane, right-click anywhere to display the context menu.

  2. Point to Alarm View settings and then click Display Alarm View on alarm .

  • Creating a Filtered Alarm View
  • Alarms Pane and Alarm View Customization
  • Alarm View Properties
  • Alarms Pane Context Menu - Alarm View Settings Submenu