The meter function adds meter properties to any trend log type to seamlessly handle consumption calculations independent of meter rollover or meter exchange.
You create and configure the meter function in trend logs using WorkStation.
For example, in the figure below, the meter function in the trend log records a meter the 1st of every month. In the middle of February, the meter rolls over to 00000. A chart with meter consumption calculation prints the consumption every month.
action_zoom_plus_stroke
Figur:
Meter trend log
The calculation function supports negative meter consumption values, which can be used to handle cases where you need to subtract consumption, for example, when energy is produced on site.
When physically replacing an old meter with a new one, you have to configure the meter function of the trend log by adding the configuration and values of both the old and the new meter. These configurations and values are the foundation when handling a meter rollover or calculating consumption though meter replacement.
Mer information finns i Managing Meter Replacement
.
action_zoom_plus_stroke
Figur:
Manage replacement of meter dialog box where you enter the values of both the old and the new meter