earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Trends
Product version: 3.2, 3.3, 2022, 2023, 2024
10/15/2020

Displaying the History of a Trend Log Record

You show the history of a trend log record, such as the original value as well as edits, through the trend log list.

Show More
action_close

​The trend log list numerically displays the records of a trend log or an extended trend log. The records of the trend log can be processed by a calculation method before they are presented in the trend log list.

The trend log list can only display one trend log at a time and must be manually refreshed to display recently recorded values.

 
action_zoom_plus_stroke Trend log list, schematic
Figure: Trend log list, schematic

You can manually add records to a trend log list for any type of trend log.

Time Zone Modes in a Trend Log List

​In a trend log list, you can present the records of a trend log in different time zones: local time zone, EcoStruxure BMS server time zone, and UTC time zone.

For more information, see Time Zone Modes in a Trend Log List .

Calculation Methods

​Use a calculation method to process the records of the trend log before presenting them in a trend log list or a trend chart. The original records in the trend log are not affected by the calculation method. The calculation method is applied to the trend log records grouped by a specific time interval.

For more information, see Calculation Methods .

Period Timestamps in Trend Charts and Trend Log Lists

When a calculated value for a period is presented, the middle of the period is used as the timestamp.

Example:

The calculated value for the period 8:00-9:00 is stamped 8:30. If there is a value at 9:01, the next period is 9:00-10:00, which is stamped as 9:30. The full period may not have passed yet, but the value can be presented even if parts of the period are in the future.

Temporary Trend Log Lists

​To display a trend log without creating a new trend log list or trend chart, the trend log can be displayed in a temporary list or chart.

For more information, see Temporary Trend Log Lists .

Floating Point Values NaN, INF, and -INF

In the EcoStruxure Building Operation software, the floating point values “Not a Number”, positive infinity, or negative infinity may be displayed in the Basic property tab, in a trend log list, or a trend chart.

For more information, see Floating Point Values NaN, INF, and –INF .

To display the history of a trend log record
  1. In WorkStation, in the System Tree pane, select the trend log list you want to show.

  2. In the Trend log list , right-click a record, and then click Show history .

  3. Click Close .

The dialog box displays all old values and which user that edited the record.

  • Editing or Commenting a Trend Log Record
  • Trend Log Lists
  • Trend Log List Context Menu