Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Editing a Backup Rule

You edit a backup rule on an EcoStruxure BMS server to change the type of data that you want to back up. You can also set up this backup rule to follow a shadow schedule that references a lead schedule managed on another EcoStruxure BMS server. 

Pokaż więcej
action_close

The EcoStruxure Building Operation scheduled backups are managed by backup rules, which are conditions that govern behavior. Similar to a scheduled task, a backup rule performs a backup on an EcoStruxure BMS server using three pieces of data: when the backup occurs, what type of data will be backed up, and a comment describing the purpose of the backup.

The EcoStruxure Building Operation software automatically backs up all data on an EcoStruxure BMS server every Sunday at 01:00. However, you can change the backup rule settings. For example, you can change the type of data you want to back up.

You can create your own backup rules to complete different tasks on different EcoStruxure BMS servers. For example, you can create a backup rule that backs up all data on the Enterprise Server twice a day rather than once a week based on the default setting. In addition, you can set up another backup rule for one EcoStruxure BMS server, which acts as the lead, to manage a recurring backup for a group of EcoStruxure BMS servers. Więcej informacji zawiera Backup Rules View .

To edit a backup rule
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Backup rules .

  4. In the Backup rules view, select a backup rule and then click the Edit backup rule button

     
    action_zoom_plus_stroke
    .

  5. In the Backup rule dialog box, in the Backup set description box, type or modify the backup comment.

  6. In the Backup content box, change the type of data you want to back up:

    • Select Configuration only to back up the configuration database and custom object type data. For example, use this option to restore data to a replaced EcoStruxure BMS server with the same name in the system.

    • Select All data to back up the configuration, historical, and custom object type data. For example, use this option to preserve the configuration and historical data for a specified date and time.

  7. In the Lead rule box, enter a backup rule that references a lead schedule managed on another EcoStruxure BMS server.

  8. In the Enabled box, select Yes to enable the backup rule.

  9. Click OK .

  10. On the File menu, click Save .

  • Backup Rules
  • Scheduled Backups
  • Deleting a Backup Rule
  • Editing a Backup Schedule
  • Backup Rules View