Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.8
13/10/2016

Editing a Backup Schedule

You edit a backup schedule, which is combined with a backup rule, to change the frequency of the backup. 

Mostrar más
action_close

Building Operation includes a digital schedule that is combined with a default backup rule. Using this schedule and rule, the system automatically backs up all data on a SmartStruxure server every Sunday at 01:00. You can change the schedule settings for this backup rule, but you cannot delete the schedule and select another.

 
action_zoom_plus_stroke Backup on a standalone Automation Server
Figura: Backup on a standalone Automation Server

You can create a custom backup rule and then modify its schedule. For example, you can create a backup rule that backs up all data on an Automation Server daily at 02:00. Para obtener más información, consulte Backup Rules View .

To edit a backup schedule
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the Enterprise server.

     
    action_zoom_plus_stroke
  3. Click Backup Rules .

  4. In the Schedule column, click the schedule that you want to modify.

     
    action_zoom_plus_stroke
  5. Revise the schedule and then click the Save button

     
    action_zoom_plus_stroke
    .

  • Backup Schedules
  • Adding a Weekly Event
  • Cómo editar un evento semanal
  • Adding a Date Exception Event
  • Editing a Date Exception Event
  • Adding a Date Range Exception Event
  • Editing a Date Range Exception Event
  • Adding a Calculated Exception Event
  • Editing a Calculated Exception Event
  • Schedule Editor ​– Basic View
  • Synchronizing SmartStruxure Server Backups on a Network
  • Backup Rules View
  • Advanced Schedule Editor – Graphic View
  • Edit Time Value Period Dialog Box