earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 时间表
产品版本: 1.8
2016/10/13

Editing a Calculated Date Calendar Event

You edit a calculated date calendar to change the information about a calendar event.

To edit a calculated date calendar event
  1. In WorkStation, in the System Tree pane, select the calendar you want to edit.

  2. In Calendar Editor , select the calculated date calendar.

     
    action_zoom_plus_stroke
  3. Right-click the calculated date calendar.

  4. Edit the properties.

     
    action_zoom_plus_stroke

    表格: Edit Calendar Entry Dialog Box - Calculated date

    Component

    Description

    Entry name

    Type an entry name for the calendar entry.

    Month

    Select a month for the exception event or Odd month , Even month , Any month .

    Week of month

    Select a week of the month for the exception event or First week , Second week , Third week , Fourth week , Last week , Any week .

    • First week – the first through the seventh day of the month. Be aware that it does not necessarily correspond to the first row of the calendar since it may include dates from both the first and second row of the calendar.

    • Fifth week – days 29 through 31 if they exist. It is always less than seven days and is non-existent in February except in a leap year.

    • Last week – the last seven days of the month. It differs from the Fifth wee k .

    Day of week

    Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting.

  5. Click OK .

  • Edit Calendar Entry Dialog Box – Calculated Date
  • Calendar Editor Overview
  • General Information Properties – Basic Tab
  • References Tab