You edit a calendar exception event to change the information about an exception event.
In WorkStation, in the System Tree pane, select the schedule containing the calendar exception event you want to edit.
Click the Basic tab.
In the calendar view, select the date when the calendar exception event you want to edit is valid.
In the event grid, select the calendar exception event you want to edit. To edit the dates for the calendar exception, you need to separately open the calendar object itself. For more information, see Editing a Date Calendar Event .
Click the Edit schedule event button
In the Schedule Event Properties dialog box, edit the properties:
Property |
Description |
Event type |
Click Exception to display the exception types. |
Exception type |
Select Calendar to initiate a calendar reference. |
All Day |
Select to create an all day event. |
![]() |
Click to add a line to the Times and values box. |
![]() |
Click to delete an entry from the Times and values box. |
Name |
Type a name for the event. |
Priority |
Select a priority number between 1 (highest priority) and 16 (lowest priority). |
Calendar |
Select a calendar to reference. |
Click OK .
On the File menu, click Save .