earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
功能: 时间表
产品版本: 2024, 7.0
2024/12/3

Editing a Date Range Exception Event

You edit a date range exception event to change the information about an exception event.

To edit a date range exception event
  1. In WorkStation, in the System Tree pane, select the schedule containing the date range exception event you want to edit.

  2. Click the Basic tab.

  3. In the calendar view, select the date when the date range exception event you want to edit is valid.

     
    action_zoom_plus_stroke
  4. In the event grid, select the date range exception event you want to edit.

  5. Click the Edit schedule event button

     
    action_zoom_plus_stroke
    .

  6. In the Schedule Event Properties dialog box, edit the properties.

    表格: Schedule Event Properties Dialog Box - Date Range Exception View

    Property

    Description

    Event type

    Click Exception to display the exception types.

    Exception type

    Select Date range for the exception to apply to the schedule.

     
    action_zoom_plus_stroke

    Click to add a line to the Times and values box.

     
    action_zoom_plus_stroke

    Click to delete an entry from the Times and values box.

    All Day

    Select to create an all day event.

    Name

    Type a name for the event.

    Priority

    Select a priority number between 1 (highest priority) and 16 (lowest priority).

    Year

    Select a year. You can use Any year as a valid entry.

    Month

    Select a month for the exception event or Odd month , Even month , Any month .

    Day of month

    Select a value for the day of the month. You can use Any Day , Last day , Odd days or Even days as valid entries.

    Day of week

    Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting.

  7. Click OK .

  • Exception Events in WorkStation
  • Adding a Date Range Exception Event
  • Schedule Event Properties Dialog Box – Date Range Exception View