earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WorkStation
Funkcje: Harmonogramy
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-11-26

Editing a Weekly Event

You edit a weekly event to change the information about a weekly event on a single day.

To edit a weekly event
  1. In WorkStation, in the System Tree pane, select the schedule you want to edit.

  2. In the Work area, click the Basic view.

  3. In the Event grid, select the weekly event you want to edit.

  4. On the Basic toolbar, click the Edit schedule event button

     
    action_zoom_plus_stroke
    .

  5. In the Schedule event properties dialog box, edit the properties.

    Tabela: Schedule Event Properties Dialog Box

    Component

    Description

    Event type

    Click Weekly to select a weekly event type.

    Days of week

    Select the days of the week that apply to this schedule.

    All Day

    Select to create an all day event.

     
    action_zoom_plus_stroke

    Click to add a line to the Times and values box.

     
    action_zoom_plus_stroke

    Click to delete an entry from the Times and values box.

  6. Click Ok .

  • Schedule Event Properties Dialog Box – Weekly View
  • Weekly Events in WorkStation