Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Alarmes
Version produit : 2024, 7.0
03/12/2024

Editing an Action Note

You edit an existing action note to change the name or the descriptions, or to add the action note to another group.

To edit an action note
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Action notes .

  4. In the Action notes view, select the action note you want to edit .

  5. Click the Edit action note button

     
    action_zoom_plus_stroke
    .

    Déclaration
    • To permanently remove an action note from the action notes list, click the Remove action note button

       
      action_zoom_plus_stroke
      .

  6. In the Edit Action Note dialog box, in the Name box, type a name for the action note.

  7. In the Group name box, type a name to create a new group or select an existing group.

  8. In the Description box, type a description for the action note.

  9. Click OK .

  10. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Alarm Control Panel – Action Notes View
  • Creating an Action Note
  • Creating an Action Note using WebStation
  • Editing an Action Note using WebStation
  • Adding an Action Note to an Alarm
  • Adding an Action Note to an Alarm using WebStation
  • Configuring Forced User Actions
  • Configuring Forced User Actions using WebStation
  • Import and Export of Supporting Objects