earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2024, 7.0
2024/12/3

Editing the Description of a Workspace

You edit the description of a workspace to specify what the workspace is used for.

显示更多
action_close

The workspace defines the content and layout of WorkStation. The content and layout of the workspace can be adapted different tasks for user accounts or user account groups.

You can create different workspaces for different user categories and link them to user account groups. A user has access to all workspaces linked to the user account groups in which the user is a member. This way, users can easily switch workspaces during a work session. For example, Paul, a member of the Administrators and Janitors user account groups, has access to the Administrator workspace and Janitor workspace.

 
action_zoom_plus_stroke Users gain access to the workspaces linked to their user account groups
图: Users gain access to the workspaces linked to their user account groups

If a user account or user account group is assigned to more than one workspace, WorkStation asks you to select a default workspace at the first log on. The next time you log on to the EcoStruxure BMS on the same computer, your default workspace is automatically displayed. Once logged in, you can change your default workspace settings. ​

Predefined Workspaces

​Some workspace layouts are included in the EcoStruxure Building Operation software and cannot be deleted or edited. Those workspaces are located in the local domain of the EcoStruxure BMS server.

有关更多信息,请参阅 Predefined Workspaces .

Workspace Components and Customization

​A workspace consists of panes, windows, and a work area that can be customized to suit a user's specific needs. Dialog boxes are presented on top of the workspace.

有关更多信息,请参阅 Workspace Components and Customization .

WebStation in Kiosk Mode

You can configure to run WebStation in Internet Explorer in kiosk mode if you want to limit the users’ access to toolbar and shortcuts in Internet Explorer.

有关更多信息,请参阅 WebStation in Kiosk Mode .

To edit the description of a workspace
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Account management .

  4. In the Domain Control Panel, in the Domain box, select the domain the workspace belongs to.

  5. In the Workspaces list, select the workspace.

  6. Click Summary .

  7. In the Summary tab, in the Description box, type a new description for the workspace.

  8. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Workspace Management
  • Control Panel Tab
  • Workspace – Summary Tab
  • Creating a Workspace