earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 1.9
2016/12/14

Editing the Path Permissions of a User Account

You edit the path permissions of an individual user account to change the access the user account has to Building Operation.

注释:
  • You cannot configure command permissions on an individual user account, only path permissions.

  • You configure command permissions on user account groups. 有关更多信息,请参阅 Software Permissions and User Account Groups .

显示更多
action_close

​Path permissions are used to give a user account group or a user account access to the objects defined in the path. The permissions configured on a path apply to all path sub-levels unless you configure new permissions for the path sub-level.

有关更多信息,请参阅 Software Permission Rules .

Example

A user has the full set of permissions: Read, Write, Create, Delete, Edit, and Force to the folder Building A. The user account group also has Read permissions to the folder Building B, but No access to the sub-folders of Building B. Therefore, the user has permission to navigate and modify the objects in the Building A folder, but only permission to view the objects in the Building B main folder.

 
action_zoom_plus_stroke Path permissions in Building Operation
图: Path permissions in Building Operation

Path Permissions Example

A user account group has the full set of path permissions to the Enterprise Server and no permissions to the Servers folder on the Enterprise Server. A single user account has the full set of path permissions to Automation Server 1, but no path permission to Automation Servers 2 and 3. Even though the user account group has no path permission to the Servers folder, it is possible to give individual user accounts access to individual Automation Servers in the Servers folder.

有关更多信息,请参阅 Path Permissions Example .

Context-Sensitive Path Permissions

You can manage permissions by configuring the permissions for a given user account or user account group to a certain object in the System Tree pane or List View and below that object, for example, a folder and its contents.

有关更多信息,请参阅 Context-Sensitive Path Permissions .

To edit the path permissions of a user account
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Account management .

  4. In the Domain list box, select the domain the user account belongs to.

     
    action_zoom_plus_stroke
  5. In the User Accounts list box, select the user account for which you want to edit path permissions.

  6. Click Software permissions .

  7. Select the path for which you want to edit the permissions.

     
    action_zoom_plus_stroke
  8. In the permissions column, select a new permission.

     
    action_zoom_plus_stroke
  9. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Path Permissions
  • Software Permissions
  • Assigning Path Permissions to a User Account
  • Removing Path Permissions from a User Account
  • User Account – Software Permissions Tab
  • Editing the Software Permissions of a User Account Group
  • Restricting the Permission to Change the Alarm State Sort Order
  • Account Management Control Panel
  • Software Permission Rules
  • Can not Access SmartStruxure Servers or Folders that You Earlier had Access to