earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Trends
Product version: 1.9
12/14/2016

Enabling a Trend Log

You enable trend log to start recording values.

Show More
action_close

​The interval trend log and change of value trend log start recording values when the configured activation conditions are met. If an activation variable is used, both the activation variable and the activation time have to be true for the trend log to start recording.

On all trend logs, you can stop recording values by disabling the trend log. To resume recording, you enable the trend log. For more information, see Disabling a Trend Log .

Activation Variable

You configure an activation variable to have the trend log start recording values when a connected variable goes on. This variable can be a scheduled variable or a variable from a switch.

You can also have the trend log stop recording when the variable, such as a fan, goes off. For example, you can use this feature to log the effective time a fan is on.

 
action_zoom_plus_stroke Activation variable that follows the activation time
Figure: Activation variable that follows the activation time

Start at activation time

You configure an activation time to have the trend log start recording values at a specified time.

For Interval Trend Logs, the logging interval is aligned with the activation time. For more information, see Interval Trend Logs .

 
action_zoom_plus_stroke Trend log that starts recording at activation time
Figure: Trend log that starts recording at activation time

To enable a trend log
  1. In WorkStation, System Tree pane, select the folder or SmartStruxure server where the trend log is located.

  2. Select the trend log you want to enable.

  3. On the Actions menu, point to Activation, and then click Enable trend log .

     
    action_zoom_plus_stroke

The trend log is now enabled and starts recording when its start condition is fulfilled.

  • Disabling a Trend Log
  • Trend Log Activation
  • Actions Menu – Activation Submenu
  • Trend Log Does Not Start Record Due to the Start Condition
  • Trend Chart Does Not Show Trend Log Series