Every time an alarm changes its state, such as from alarm state to reset state, an event is written in the event log and shown in the Events pane in WorkStation. You can disable state-change logging if you are only interested in the current alarm status. For example, you want to present the current alarm status in a graphic and do not care about the event history.
Count
In the Alarm view, the value in the Count column counts +1 each time an alarm changes to alarm state. When the alarm state changes to normal, the count is reset to zero.
For more information, see Count
.