earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Como

Como


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Gestão de utilizadores
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Forcing a User to Change the Password at Next Logon

You force a user to change the password at next logon to increase the security, for example, when distributing a user account to a new user.

Mostrar mais
action_close

As a WorkStation administrator, you can change users’ passwords, force users to change their passwords at next logon, or enable and disable the possibility for users to change their passwords.

Passwords are managed at the user account group level. EcoStruxure Building Operation software applies password changes to all user accounts that belong to the user account group.

Nota
  • If you are an administrator and have forgotten your password, contact the EcoStruxure BMS support team.

To force a user to change the password at next logon
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Account management .

  4. In the Domain list box, select the domain the user account belongs to.

  5. In the User Accounts list, select the user account.

  6. Click Summary .

  7. In the Force password change box, select True to force the user to change the password at next logon.

  8. Click the Save button

     
    action_zoom_plus_stroke
    .

The Force password change box is automatically set to False when the user changes their password.

  • User Accounts and User Account Groups
  • Control Panel Tab
  • User Account – Summary Tab
  • Password Administration
  • Password Policy