earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.9
14/12/2016

General Information Properties – Basic Tab

Use the Basic tab to configure and view the General Information properties.

 
action_zoom_plus_stroke General Information properties – basic tab
Figura: General Information properties – basic tab

Tabla: General Information Properties

Component

Description

Name

​Displays the name of the object.

Description

Type a description that explains what the object is used for.

Type

​Displays the object type that defines the properties of the object.

Foreign address

Displays the address to a non-Building Operation device, for example a BACnet device.

Modified

​Displays the date and time when the object was last modified.

Note 1

Type text that you display in a graphic or use when searching for the object.​

Note 2

​Type text that you display in a graphic or use when searching for the object.

Validation

Select the validation status of the object to keep track of which objects have passed or failed the validation.

Executed by

Indicates the object is executed by a BACnet device. An empty field indicates the object is executed by an Automation Server or Enterprise Server.

  • Object Properties
  • References Tab