earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.9
25/03/2017

Object Properties

Every object in Building Operation has a number of different properties. Properties can be of two different types: read only and read/write. Read only properties are dimmed and cannot be changed. Read/write properties can be changed.

There are three ways to access the properties of a selected object in WorkStation:

  • Properties tab

  • Properties Dialog box

  • Properties grid

All three methods displays the same properties.

 
action_zoom_plus_stroke The Properties tab for a trend log.
Figura: The Properties tab for a trend log.

The properties are sorted under different tabs in the properties tab/dialog/grid. The number of tabs depends on the object. Some object have a lot of properties and tabs, others have only one tab with only a few properties.

 
action_zoom_plus_stroke A SmartStruxure server object with three properties tabs (left) and a value with only the basic properties tab.
Figura: A SmartStruxure server object with three properties tabs (left) and a value with only the basic properties tab.

A common tab for all objects is the Basic properties tab that contains general properties as type, name and description.

  • Building Operation Objects
  • Multi-edit
  • Editing Multiple Objects
  • General Information Properties – Basic Tab