Produkty: WorkStation
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-10-23

Help Menu – Help Settings Submenu

Use the Help Settings submenu to select the help you want to use.

 
action_zoom_plus_stroke Help Settings submenu
Rysunek: Help Settings submenu

Tabela: Help Settings Submenu

Command

Description

Automatic

Click to make WorkStation check if you are connected to the Internet. If you are connected, WebHelp opens. If you are not connected, the System Reference Guide opens.

Building Operation help

Click to always open WebHelp. If you are not connected to the Internet, you get an error message.

Building Operation guide

Click to always open the System Reference Guide, regardless of whether you are connected to the Internet or not.

  • WorkStation Help
  • Help Menu