Produkty: Enterprise Server, Function Block Editor, Graphics Editor, License Administrator, License Server, Script Editor, Software Administrator
Funkcje: Podstawowa funkcjonalność, Aktualizacja
Wersja produktu: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Installation Wizard – License Server Configuration Page

Use the License Server Configuration page to configure the address to the license server.

 
action_zoom_plus_stroke License server configuration page
Rysunek: License server configuration page

Tabela: License Server Configuration Page

Component

Description

License Server Address

Type the address to the license server where licenses are available for check out. The address must begin with @. To define the port number, if other than the default port range 27000-27009, type the port number in front of the @, Port-number@Address. Use a semicolon to separate addresses.

  • Installation Overview
  • Server Installation Wizard – Configuration Page
  • Installation Wizard – Choose Components Page
  • Installation Wizard – Installation Type Page
  • License Administrator