You install the Enterprise Server to collect data throughout the EcoStruxure BMS while providing supervisory control.
Ensure that you have a working and available Enterprise Server license. A working license is required to start the Enterprise Server. For more information, see EcoStruxure Building Operation Software Licensing Installation and Location .
In Windows, disable any anti-virus program.
Double-click on the Enterprise Server installation file to start the installation wizard.
If User Account Control (UAC) is enabled, you must run the installer as administrator. Right-click the installation file and then click Run as administrator .
Click Yes to confirm that you want to run the installation package.
Click Next .
Make sure that you agree with the End User License Agreement (EULA) and then click I Agree .
Browse to the folder where you want to install the Enterprise Server and then click Next .
When upgrading to a later version, the installation path is changed to the default installation folder for that version. The default installation folder is always located on the C: drive
The complete installation path can have maximum 115 characters.
EcoStruxure Building Operation products are installed in the same folder that you selected for the first product you installed
In the Database Folder box, enter the path to the location where you want to save the Enterprise Server database.
The database folder path can contain up to 140 characters.
Click Next .
In the HTTP Port box, type the port number the Enterprise Server listens to when communicating through the Hypertext Transfer Protocol.
In the HTTPS Port box, type the port number the Enterprise Server listens to when communicating through the Hypertext Transfer Protocol Secure.
In the TCP Port box, type the port number the Enterprise Server listens to when communicating through the Transmission Control Protocol.
Click Next .
Select Local system to run the Enterprice Server service under the Local system account.
For security reasons, it is recommended that you run the Enterprise Server service under a custom Windows user account with limited permissions.
To run the Enterprise Server service under a custom Windows account, select Custom, enter the domain and user account names, click Verify Account to verify that the account exists, and then type the user account password.
To be able to log on to WebStation, the selected Windows user account has to have write permissions to C:\Program Files (x86)\Schneider Electric EcoStruxure\Building Operation X.X\Enterprise Server.
In the License Server Address box, type @ and then type the address to the License Server.
If the License Server uses a port other than the default port range 27000-27009, type the port number in front of @. For example, 567@localhost.
Use a semicolon to separate addresses to different License Servers.
Click Next .
Revise the information on the Summary page and then click Install .
Click Next .
Click Show details to follow the progress of the installation.
Click Finish .
In Windows, enable any anti-virus program.
When the installation is completed, make sure that the HTTP port, HTTPS port, and TCP port are not used exclusively by any other application.
In case of a port conflict, users are not able to log on to the EcoStruxure BMS. In Software Administrator, resolve any port conflict. For more information, see Resolving Enterprise Server or Enterprise Central Port Conflicts ..