The License Administrator administers the activation, return, and repair of licenses.
You use License Administrator to activate EcoStruxure Building Operation software licenses on the License Server. The licenses are then checked out from the License Server by WorkStation, editors, or Enterprise Server. Более подробную информацию см. License Administrator .
During the installation of License Administrator on WorkStations or Enterprise Servers, you can change the the network address to the License Server where licenses are available for check out. The address to the License Server can later be entered or edited through License Administrator on the computer that hosts the licensed product.
When you use the default setting during installation, you do not have to change the network address. Более подробную информацию см. EcoStruxure Building Operation Software Licensing Installation and Location .
The address to a License Server must begin with @ and is either a hostname or IP address. If the communication to the License Server is through a port other than the default port range 27000-27009, the port number is defined in front of the @, Port-number@hostname.
Address |
Description |
19650@localhost |
Connects to localhost through port 19650 |
@server2c.schneider-electric.com |
Connects to License Server server2c.schneider-electric.com through a port in the default port range 27000-27009 |
14650@192.166.248.2 |
Connects to License Server 192.166.248.2 through port 14650 |
To separate License Server addresses in License Administrator, use a semicolon.