earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 3.1
2022/12/14

License Management

The EcoStruxure Building Operation license system consists of, for example, a License Server, WorkStation with client tools, and the Enterprise Server. The number of each component varies depending on the system size and architecture.

In this example, the License Server and Enterprise Server are located on the same computer. Several WorkStations check out licenses from the License Server through the local area network. Network licenses are activated on the License Server by the License Activation Server that is controlled by Schneider Electric.

 
action_zoom_plus_stroke WorkStation system with License Server and Enterprise Server on same computer and WorkStation in separate computers, one computer with client tool.
图: WorkStation system with License Server and Enterprise Server on same computer and WorkStation in separate computers, one computer with client tool.

License System Installation and Configuration

Schneider Electric recommends that you install the license server framework before installing other EcoStruxure Building Operation software applications and SmartX servers. The license server installation is included in the License Administrator license package. During the installation of WorkStation or Enterprise Server, the installation software asks for the address to the license server.

有关更多信息,请参阅 Installation Example .

Network License Management

When you activate a license, the license is transferred from the License Activation Server to your License Server. When activating a license, details about the transaction and registration details are stored with the license on the License Server.

有关更多信息,请参阅 Network License Management .

  • Licensing Overview
  • Network License Management
  • Local License Management
  • Installation Example