earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Device Administrator, Enterprise Central, Enterprise Server, Function Block Editor, Graphics Editor, ​License Administrator, ​License Server, AS-P, Script Editor, Software Administrator
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Installation Example

Schneider Electric recommends that you install the license server framework before installing other EcoStruxure Building Operation software applications and SmartX servers. The license server installation is included in the License Administrator license package. During the installation of WorkStation or Enterprise Server, the installation software asks for the address to the license server.

License files used to activate time-limited local licenses can be distributed under certain circumstances.

有关更多信息,请参阅 Local Licenses .

注释:
  • Plan the license management carefully and purchase network licenses early to avoid unexpected operational stops caused by expired local licenses.

This work flow describes an EcoStruxure BMS where license server and Enterprise Server are located on the same computer.

To install the EcoStruxure Building Operation software smoothly use the following installation order:

 
action_zoom_plus_stroke Installation and configuration order
图: Installation and configuration order

表格: Installation and Configuration Order

Number, client/server

Description

1. License Server

  • Install the License Server and License Administrator.

  • When the License Administrator installation wizard prompts, type the address to the license server. In this case, type @localhost.

  • Activate network licenses, on the license server. 有关更多信息,请参阅 Network License Management .

  • Note the ​network address of the license server.

2. Enterprise Server

  • Install the Enterprise Server.

  • When Enterprise Server installation wizard prompts, type the address to the license server.

  • Optional: Install License Administrator to edit the address to the license server or activate a local license.

3. Workstation

  • Install WorkStation together with the bundled tools.

  • When WorkStation installation software prompts, type the address to the license server.

  • Optional: Install language packages.

  • Optional: Install License Administrator to edit the address to the license server or activate a local license.

4. other applications

  • Install Device Administrator.

  • Install Reports.

If network licenses are not purchased or are missing, local licenses can be activated from license files. Replace local licenses with purchased licenses before the local licenses expire.

  • Licensing Overview
  • Installing WorkStation and Client Tools
  • Installing the Enterprise Server
  • Installing the License Administrator and the License Server
  • Installing the Device Administrator
  • License Management
  • Installing a Language Pack
  • Network License Management
  • Local Licenses
  • Installation Overview