earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 1.8, 1.9
2016/2/5

License Server Maintenance

Building Operation licenses are controlled by license policies regarding the transaction of licenses. Therefore, it is important that a replacement or reinstallation of the license server is carefully planned.

License Server Address Change

If the License Server is assigned a new network address, all WorkStations and Enterprise Servers must be updated with the new address.

License Server Reinstallation

When reinstalling a License Server, the licenses on the License Server are not affected. All you have to do is to uninstall the License Server and then reinstall it. The licenses on the License Server do not have to be returned to the License Activation Server.

License Server Replacement

Before replacing the License Server hardware, return the licenses to the License Activation Server and then activate the licenses on the new License Server.

You can also use this workflow when relocating licenses to another License Server.

 
action_zoom_plus_stroke Replacing the License Server or moving licenses
图: Replacing the License Server or moving licenses

表格: Replace of Licenses or Move of Licenses

Number

Description

1

All licenses, located on the old License Server, are returned to the License Activation Server.

2

The License Activation Server activates the licenses on the new License Server using the entitlement ID that originally was used to activate the licenses.

Make sure that the new License Server has the same network address as the former License Server. If a new network address is assigned, update all WorkStations and Enterprise Servers with the address to the new License Server.

License Server Reset

If problems with the License Server or activated licenses occur, you may have to reset the License Server. All details about activated licenses on the License Server are compiled in files that start with "taclic" and have the .data extension. The file name string after "taclic" can differ. An example of the License Server file name is taclic_00249e00_tsf.data. The license details files are created the first time a license is activated on the License Server. By deleting the files you reset the License Server.

有关更多信息,请参阅 License Server Reset .

  • Licensing Overview
  • License Administrator
  • Starting the License Server
  • Stopping the License Server
  • Restarting the License Server