earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
5
概念

概念


产品: ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 1.8, 1.9
2015/5/28

License Administrator

arrow1_rotationRegistration Details arrow1_rotationLicense Server Address

The License Administrator administers the activation, return, and repair of licenses.

Registration Details

Before the first network license is activated on the License Server, details about the customer’s organization and the contact information of the account manager must be entered. The registration details are written to the license details when a license is activated. Building Operation automatically saves these registration details and reuses the details the next time a license is activated.

注释:

​Only English letters are allowed in the license details.

If you change the registration details, the changes are applied to all licenses located on the License Server.

注释:
  • To ensure that all the licenses have the same information, the registration details must be updated on all License Servers in the Building Operation system.

License Server Address

​During the installation of License Administrator on WorkStations or Enterprise Servers, you need to type the network address to the License Server where network licenses are available for check out. The address to the License Server can later be entered or edited through License Administrator or directly in the Windows registry ​of the computer or Enterprise Server that hosts the licensed product.

有关更多信息,请参阅 ​License Server Address .

  • Licensing Overview
  • License System
  • Licenses
  • Registration Details View
  • Licenses View Icons
  • License Server Address View
  • Diagnostics View
  • Editing Registration Details
  • Activating Network Licenses
  • Activating a Local License
  • Removing a Local License or Returning a Network License
  • Viewing Activated Licenses
  • Repairing a Network License
  • ​License Server Address