License Server manages the administration of EcoStruxure Building Operation software licenses.
An EcoStruxure BMS running with EcoStruxure Building Operation Software licenses must contain at least one License Server. Use one License Server on every computer that runs a feature that require an EcoStruxure Building Operation software license.
License Server is a Microsoft Windows service named Building Operation License Server.
Configure the License Server to automatically restart if it unexpectedly stops. For more information, see Configuring the License Server Recovery Settings .
You can access License Server through a web interface. For more information, see Accessing License Server Using the Interface .
With a default installation, the License Server port range is set to 27000-27009. A valid number is any unused port between 0 and 64000.
If the License Server uses other ports than the default port range 27000-27009, the port has to be added in front of the @ in the License Server address on the WorkStation, Enterprise Server, or Client tools.