earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2.0, 2.1, 3.0, 3.1
26/06/2018

Local Backup and Restore of EcoStruxure BMS Servers

In WorkStation, you can log on to an EcoStruxure BMS server directly to perform manual backup and restore tasks.

Local Backup and Restore of a Standalone SmartX Server

In WorkStation, you can log on to a SmartX server to perform a manual backup of the SmartX server data.

If you have multiple standalone SmartX servers, the Backup and Restore processes on one SmartX server remain self-contained and, therefore, separate from any another SmartX server on the network.

In a stand-alone system only one backup set is stored on the SmartX server. If you import a backup set, the system overwrites the locally stored file with the imported file. Therefore, you only see one backup file in the Restore Options dialog box when you log on to a SmartX server.

Local Backup and Restore of an Enterprise Server

In WorkStation, you can log on to an Enterprise Server to perform a manual backup of the Enterprise Server data. If you have multiple Enterprise Servers, the Backup and Restore processes on one Enterprise Server remain self-contained and, therefore, separate from any another Enterprise Server on the network.

Local Backup and Restore of an Enterprise Central

In WorkStation, you can log on to an Enterprise Central to perform a manual backup of the Enterprise Central data. The Backup and Restore processes on Enterprise Central are self-contained.

  • Manual Backups
  • Backup Sets
  • Backup Set Properties – Basic Tab