earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: Device Administrator, License Administrator, License Server
Funkcje: Zarządzanie licencją
Wersja produktu: 2022
2023-02-21

Demo Licensing Overview

Demo licenses are used for demonstration purposes, training, or when building a site.

There are two types of demo licenses:

  • EcoStruxure Building Operation Software Demo Licenses on Windows. These licenses are managed by License Administrator and handles licenses on Enterprise Server and Enterprise Central.

  • SpaceLogic Automation Server Demo Licenses. These licenses are managed by Device Administrator and handles licenses on Automation Servers.

EcoStruxure Building Operation Software Demo License on Windows Management

Demo licenses for EcoStruxure Building Operation software are local, bound to the computer, and cannot be shared.

The license file used to activate demo licenses can only be used once per computer and is time-limited. The demo license is installed on License Server from a license file with the extension .asr. Demo licenses must be activated on the same computer that runs WorkStation, Enterprise Server or Enterprise Central.

Więcej informacji zawiera EcoStruxure Building Operation Software Demo Licenses on Windows Management .

SpaceLogic Automation Server Demo License Management

You add and return licenses on automation servers using Device Administrator.

Więcej informacji zawiera SpaceLogic Automation Server Demo License Management .

  • Licensing Overview
  • Demo Licensing Overview
  • EcoStruxure Building Operation Software Licensing Overview
  • EcoStruxure Building Operation Software Demo Licenses on Windows Management
  • SpaceLogic Automation Server Demo License Management