earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: Edge Server, Device Administrator, ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 2024
2024/12/3

Demo Licensing Overview

Demo licenses are used for demonstration purposes, training, or when building a site.

There are two types of demo licenses:

  • EcoStruxure Building Operation Software Demo Licenses on Windows. These licenses are managed by License Administrator and handles licenses on Enterprise Server and Enterprise Central.

  • Field server Demo Licenses. These licenses are managed by Device Administrator and handles licenses on field servers.

EcoStruxure Building Operation Software Demo License on Windows Management

Demo licenses for EcoStruxure Building Operation software are local, bound to the computer, and cannot be shared.

The license file used to activate demo licenses can only be used once per computer and is time-limited. The demo license is installed on License Server from a license file with the extension .asr. Demo licenses must be activated on the same computer that runs WorkStation, Enterprise Server or Enterprise Central.

有关更多信息,请参阅 EcoStruxure Building Operation Software Demo Licenses on Windows Management .

Field Server Demo License Management

You add and return licenses on field servers using Device Administrator.

有关更多信息,请参阅 Field Server Demo License Management .

  • Licensing Overview
  • Demo Licensing Overview
  • EcoStruxure Building Operation Software Licensing Overview
  • EcoStruxure Building Operation Software Demo Licenses on Windows Management
  • Field Server Demo License Management