Productos WorkStation, WebReports
Funcionalidades: Informes
Versión del producto: 1.8, 1.9
27/05/2014

Inicio de sesión en WebReports

Puede acceder sesión en el sitio web de WebReports si desea ver y personalizar informes usando su navegador web. Si se conecta con una cuenta de administrados, también puede crear planificaciones, cargar imágenes, crear paquetes de informes, cambiar el nombre a los informes personalizados y eliminarlos, y asignar plantillas para usarlas con los informes predeterminados.

Mostrar más
action_close

You create and configure user accounts for the WebReports Web site in WorkStation. User accounts that have access to WorkStation also have access to the WebReports Web site. User accounts that do not have access to WorkStation, or whose accounts have expired, do not have access to the WebReports Web site. By default, all user accounts that have access to WorkStation, can run, view, and customize reports in WorkStation and at the WebReports Web site. When you access WebReports through the WebReports Web site, you can perform administrative tasks in addition to viewing and creating reports. To perform the administrative tasks, your user account needs to belong to the Reports Administrators user group.

The user group and user account that pertain specifically to WebReports include the Reports Administrators user group and the SystemReportsService user account.

 
action_zoom_plus_stroke  WebReports user account and user group
Figura: WebReports user account and user group
Aviso

Users who are not members of the local domain cannot by default access the administrative features of WebReports. To enable WebReports administrative access for users in a non-local domain, create a new user group called "Reports Administrators" in the non-local domain, and then add the user(s) to the new group. Para obtener más información, consulte Creating a User Account Group .

Reports Administrators User Group

User accounts that belong to the Reports Administrators group can access the reports administration pages in WebReports. You assign user accounts to the Reports Administrators group when the user account needs to perform any of the following tasks:

  • Assign a report template to a System Object type

  • Preview, delete, or upload images

  • Upload or download report packs

  • Schedule dashboard reports to run at specified times

  • Rename or delete custom reports

The Reports Administrators group does not have a Workspace associated with it. Consequently, any user account that belongs to the Reports Administrators user group is required to also belong to another group that has a Workspace associated with the group. For example, suppose you create a user account and assign the user account to the Administrators group. As a result, the user account is assigned to a group that has a Workspace associated with the group. You can now assign the user account to the Reports Administrators group to provide the user with access to the reports administration pages in WebReports. Para obtener más información, consulte WebReports Main Page .

Reports User Account

The Reports user account allows the Reporting Agent service to log on to the Enterprise Server. This user account is configured in the Reports Server during the installation of Reports. If you change the password of the Reports user account in the Enterprise Server, you need to configure the same password in the Reports Server to establish communication between the Enterprise Server and the Reports Server.

Para obtener más información, consulte Configuring Reports User Account .

Summary

The table describes the WebReports groups and users.

Tabla: WebReports User Groups and User Accounts

Groups and Users

Description

Reports Administrators Group

Allows members of the group to create custom reports, generate and view reports, and access the reports administration pages in WebReports.

Default groups such as the Administrators Group

Allows members of the group to create custom reports, and generate and view reports.

Reports User

Identifies the user name for the ES Reader service. Allows the ES Reader service to log on to the Enterprise Server.

Para iniciar sesión en WebReports
  1. En la barra de direcciones de su navegador web, introduzca la URL de WebReports, por ejemplo: http://10.159.17.246/SchneiderElectric/WebReports.

  2. En el cuadro de diálogo Nombre de usuario, introduzca su nombre de usuario de WorkStation.

     
    action_zoom_plus_stroke
  3. En el cuadro de diálogo Contraseña, introduzca su contraseña de WorkStation.

  4. En el cuadro de diálogo Dominio, introduzca un nombre de dominio. Si no introduce ningún nombre de dominio, se conectará al dominio local.

  5. Seleccione Recordarme para guardar su nombre de usuario.

  6. Haga clic en Iniciar sesión .

  • WebReports User Accounts
  • WebReports Log On Dialog Box