earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Matching Text String Alarm Properties – Basic Tab

Use the Basic tab to view or edit the basic properties of a matching text string alarm.

 
action_zoom_plus_stroke Basic tab
Figura: Basic tab

Tabla: Basic Tab

Component

Description

Alarm state

​Displays the present state of the alarm. Para obtener más información, consulte Alarm States .

Basic evaluation state

Displays False when the alarm is in its normal state.

Evaluation state

​Displays the present evaluation state of the alarm. For example, Upper limit alarm is displayed when the monitored value reaches the upper alarm limit.

Disabled cause

Displays the cause for the alarm being disabled:

  • Shunt variable means that the alarm has been disabled by a shunt variable

  • User means that the alarm has been disabled by the user

  • System means that the alarm has been disabled by the system

Monitored variable

​Enter the path to the variable that is monitored by the alarm.

 
action_zoom_plus_stroke

Add

Click to create a new alarm trigger item. Para obtener más información, consulte Create Object Dialog – Naming the Object Page .

 
action_zoom_plus_stroke

Edit

Click to edit the alarm trigger item. Para obtener más información, consulte Alarm Trigger Properties – Value tab .

 
action_zoom_plus_stroke

Remove

Click to remove an alarm trigger item.

Reset delay (s)

​Enter the time, in seconds, the alarm has to be within the reset criteria before the alarm state is changed from alarm to reset.

Para obtener más información, consulte Time Delay .

Alarm delay (s)

​Enter the time, in seconds, the alarm has to be within the alarm criteria before the alarm is triggered.

Para obtener más información, consulte Time Delay .

Shunt variable 1

​Enter the shunt variable that is used to enable or disable the alarm. Para obtener más información, consulte Shunt Variables .

Invert shunt value 1

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Para obtener más información, consulte Shunt Variables .

Shunt operator

Select AND or OR to add logic between the first and the second shunt variable. Para obtener más información, consulte Shunt Variables .

Shunt variable 2

​Enter the second shunt variable that is used to enable or disable the alarm. Para obtener más información, consulte Shunt Variables .

Invert shunt value 2

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. Para obtener más información, consulte Shunt Variables .

  • Matching Text String Alarms
  • Matching Text String Alarm Properties – Alarm Settings Tab
  • References Tab
  • Create Object Dialog – Naming the Object Page
  • Alarm Trigger Properties – Value tab
  • Alarm States
  • Time Delay
  • Shunt Variables