earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.9
14/12/2016

Editing Multiple Objects

You can edit more than one object at the same time to save time.

Mostrar más
action_close

Use Multi-edit when you want to change several property values at a time. For example, you want to change all setpoints from 22 to 20. You select all the objects in the List View, open the Properties grid, and then change the value in the Value box. You need to click Save for the changes to take effect.

 
action_zoom_plus_stroke Multi editing
Figura: Multi editing

The objects do not need to be of the same type to be edited. However, the properties you want to edit have to be of the same type.

To edit multiple objects
  1. In WorkStation, in the List View , select the objects you want to edit.

  2. In the List View , expand Properties .

  3. In the Properties grid, edit the property you want to change for all selected objects.

  4. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Multi-edit
  • List View Toolbar