earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.9
14/12/2016

Multi-edit

Use Multi-edit when you want to change several property values at a time. For example, you want to change all setpoints from 22 to 20. You select all the objects in the List View, open the Properties grid, and then change the value in the Value box. You need to click Save for the changes to take effect.

 
action_zoom_plus_stroke Multi editing
Figura: Multi editing

The objects do not need to be of the same type to be edited. However, the properties you want to edit have to be of the same type.

  • Editing Multiple Objects
  • Object Properties