earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 警报
产品版本: 1.8
2016/10/13

Create Alarm Wizard – Attachment Page

Use the Attachment page to add attachments to the alarm.

 
action_zoom_plus_stroke Attachment page
图: Attachment page

表格: Attachment Page

Component

Description

 
action_zoom_plus_stroke

Add attachment 

Click to add an attachment to the alarm. 有关更多信息,请参阅 报警附件 .

 
action_zoom_plus_stroke

Remove attachment  

Click to remove an attachment.

 
action_zoom_plus_stroke

Navigate to 

Click to open the attachment that is selected in the attachment list.

Display on alarm

Select to display the attachment when the alarm is triggered.

  • Alarm Functions
  • Create Object Wizard – Naming the Object Page
  • Create Alarm Wizard – Presentation Page
  • Create Alarm Wizard – User Action Page