earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 警报
产品版本: 1.8
2016/10/13

Create Alarm Wizard – User Action Page

Use the User Action page to force a user to actions that are connected to the alarm.

 
action_zoom_plus_stroke User Action page
图: User Action page

表格: User Action Page

Component

Description

Acknowledgement type

​Select the type of acknowledgement for the alarm.

有关更多信息,请参阅 Acknowledgements .

Cause note group

​Enter the cause note group that is used by the alarm.

Action note group

​Enter the action note group that is used by the alarm.

Checklist

​Enter the checklist that belongs to the alarm.

Required user action

​Select what actions the user has to perform when any of the listed events occur.

  • Alarm Functions
  • Create Object Wizard – Naming the Object Page
  • Create Alarm Wizard – Presentation Page
  • Create Alarm Wizard – Attachment Page
  • Comments
  • Cause Notes
  • Action Notes
  • Checklists
  • 隐藏和禁用
  • 报警指定