earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Create Alarm Wizard – Presentation Page

Use the Presentation page to configure the presentation settings of the alarm.

 
action_zoom_plus_stroke Presentation page
Figura: Presentation page

Tabla: Presentation Page

Component

Description

Above upper limit message

​Type the message to display when the variable exceeds the upper limit of the alarm.

Below lower limit message

​Type the message to display when the variable falls below the lower limit.

Alarm message

Type the message to display when the alarm is in Alarm state.

Para obtener más información, consulte Alarm Messages .

Reset message

​Type the message to display when the alarm is reset.

Para obtener más información, consulte Alarm Messages .

Category

​Enter the category the alarm belongs to.

Para obtener más información, consulte Alarm Categories .

Category 2

Enter the second category the alarm belongs to.

Para obtener más información, consulte Alarm Categories .

Prefix for alarm source name

Add a substitution code or type a prefix that is added to the beginning of the source name property of an alarm record.

Para obtener más información, consulte Alarms Substitution Codes .

Above upper limit priority

​Enter the priority level of the alarm when the variable exceeds the upper limit.

Para obtener más información, consulte Alarm Priority .

Below lower limit priority

​Enter the priority level of the alarm when the variable falls below the lower limit.

Para obtener más información, consulte Alarm Priority .

Alarm priority

Enter the priority level of the alarm.

Para obtener más información, consulte Alarm Priority .

Reset priority

​Enter the priority level of the alarm when it is reset.

Para obtener más información, consulte Alarm Priority .

Same priority

Select to set all priorities to the same value.

Para obtener más información, consulte Alarm Priority .

Auto hide

Select to automatically hide the alarm in the Alarms pane or Alarm View.

Flashing alert

Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered.

Audible alert

Select to make the alert audible when the alarm is triggered.

Custom audio

Enter the path to the custom audio file you to play when the alarm is triggered.

Para obtener más información, consulte Custom Audible Alarm Alerts .

Disable state-change logging

Select to prevent an alarm state change from creating an event.

  • Alarm Functions
  • Create Alarm Wizard – User Action Page
  • Create Alarm Wizard – Attachment Page
  • Create Object Dialog – Naming the Object Page
  • Alarms Substitution Codes
  • Alarm Messages
  • Alarm Categories
  • Alarm Priority
  • Custom Audible Alarm Alerts