Use the User actions page to force a user to actions that are connected to the alarm.
Component |
Description |
Acknowledgement type |
Select the type of acknowledgement for the alarm. For more information, see Acknowledgements . |
Cause note group |
Enter the cause note group that is used by the alarm. |
Action note group |
Enter the action note group that is used by the alarm. |
Checklist |
Enter the checklist that belongs to the alarm. |
Required user action |
Select what actions the user has to perform when any of the listed events occur. |