earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.9
22/02/2017

Non-Validated Programs Search Example

​You want to find the programs that are not validated in your system. So you search for all programs that have validation set to None or Failed.

You only want to search in University X, so you ​right-click University X and then click Search. You want to find all programs that are not validated regardless of their names. The Search box cannot be empty and you want to find all programs regardless of their names so you have to enter an asterisk (*).

 
action_zoom_plus_stroke The Search View when you have entered an asterisk (') that finds all objects in University X
Figura: The Search View when you have entered an asterisk (') that finds all objects in University X

​To narrow you search so that only program, Script or Function Block is found, you have to add Programs in the Select types dialog box.

 
action_zoom_plus_stroke The Select types dialog box when all objet types of the categories Plain English and Function Block is selected.
Figura: The Select types dialog box when all objet types of the categories Plain English and Function Block is selected.

Then you select the conditions for the search in the Select Conditions dialog box. We only want to find non-validated programs. Therefore we choose Validation from the Add condition list, and then we select None and Failed, and click OK.

 
action_zoom_plus_stroke The validation conditions None and Failed is selected in the Select Condition dialog box.
Figura: The validation conditions None and Failed is selected in the Select Condition dialog box.

Then we perform the search.

 
action_zoom_plus_stroke The search result for all program in University X that are not validated successfully
Figura: The search result for all program in University X that are not validated successfully

To be able to use the search again without going through all the settings once more we save the search with the name "Non-Validated Program Search".

  • Search Overview
  • Advanced Search
  • Search View
  • Select Folder Dialog Box
  • Select Types Dialog Box
  • Select Conditions Dialog Box
  • Searching for Objects Using Advanced Search
  • Saving a Search